CHERNE Plumbing Test Ball Plugs, Single Size
Cherne underground Test-Ball plugs are designed to block flow in sanitary and storm sewer systems, allowing easy maintenance. These plugs can also serve as a backstop for sewer air tests.
stil | Model | Nominal Boyut | Aralık | Maks. Alan sayısı Geri basınç | Gerekli Şişirme Basıncı | Sönük Çap | Sönük Uzunluk | Ücret | |
---|---|---|---|---|---|---|---|---|---|
A | 270008 | 0.75 "1.25 için" | 0.75" ila 1.3" | 17 psi/40 fit | 65 psi | 0.73 " | 3.75 " | €68.04 | |
A | 270016 | 1.25 "1.5 için" | 1.17" ila 1.75" | 13 psi/30 fit | 40 psi | 1.1 " | 5.5 " | €52.89 | |
A | 270024 | 2" | 1.9" ila 2.25" | 13 psi/30 fit | 40 psi | 1.77 " | 2.84 " | €64.68 | |
A | 270108 | 2.5 " | 2.34" ila 2.75" | 13 psi/30 fit | 35 psi | 2.3 " | 4.5 " | €67.32 | |
A | 270032 | 3" | 2.77" ila 3.25" | 13 psi/30 fit | 35 psi | 2.64 " | 5.25 " | €70.48 | |
A | 270040 | 4" | 3.41" ila 4.25" | 13 psi/30 fit | 30 psi | 3.25 " | 6.5 " | €82.43 | |
A | 270059 | 5" | 4.6" ila 5.25" | 13 psi/30 fit | 30 psi | 4.5 " | 7.75 " | €160.76 | |
A | 270067 | 6" | 5.44" ila 6.25" | 13 psi/30 fit | 30 psi | 5.25 " | 9" | €219.73 |
Özellikler
- These plugs are made of natural rubber for expansion and memory.
- They seal both round and out-of-round pipes.
- The removable inflation valve can be replaced with a quick disconnect fitting.
- These units come with an eye-bolt for use with a poly-lift line.
Standartlar ve Onaylar
- OSHA
Sık Sorulan Sorular
What is the difference between a Test Ball and a Muni Ball?
- A Test Ball does not have a bypass and is only intended to block (seal) a pipe.
- A Muni Ball has a bypass tube that runs through the plug, allowing the user to bypass effluent through the tube or complete an air test with an adapter cap.
- Muni Balls can also be used to obstruct pipes.
How to install Cherne Test-Ball plugs?
- Place the plug in the pipe or application to be blocked or tested, making sure it is at least as long as the pipe diameter.
- Connect one end of the inflation hose to a plug inflation fitting (such as a Schrader valve, 1/4, 3/8 / 1/2-inch port). The other end of the inflation hose is connected to line pressure, a pump or another source of pressure.
- Connect a second hose to the fitting if another one is available. The other end of the second hose should be connected to a gauge that has been calibrated.
- Before inflating the plug, use the appropriate method to block / brace it.
- Apply pressure to the plug using the inflation hose. Fill the plug to the inflation pressure specified on the plug.
- Allow the plug to settle for a few moments. If necessary, add pressure to maintain the rated inflation pressure.
- Continue testing the pipe / application. Once done, release back pressure behind the plug outside the danger zone.
- After releasing back pressure, relieve plug pressure from outside the danger zone until the plug is completely deflated.
- Take down the blocking / bracing system. Finally, take the plug out of the pipe.
What is the maximum temperature that these plugs can handle?
0 ila 125 Fahrenheit derece arasındaki sıcaklıkları kaldırabilirler.
Yardım etmek için buradayız!
Burada listelenmeyen bir parça mı arıyorsunuz?
Daha keşfedin
- Tambur Kaldırıcılar
- Kol ve Yüksük Kitleri
- Negatif Hava Makinaları
- Hidrolik Valf Egzersizleri
- Süzgeç
- Ayakkabı ve Ayakkabı Aksesuarları
- Zamanlayıcılar
- Uzatma Kabloları ve Çıkış Şeritleri
- Dağıtım Tabancaları
- Pirinç
- HUSKY Palet Raf Koruyucu
- SPYDER Arbor Uzantıları
- MILWAUKEE Chuck Anahtar Tutucu
- GRAINGER Black Steel Schedule 40 Kaynaklı Nipel
- BUSSMANN FWA A / B 150V Serisi Özel Sigortalar
- WILKERSON 18 ve 28 Serisi Modüler Üniteler için Marangoz Seti
- DIXON PD Serisi Fişler
- DAYTON Ön Ayaklar,PK 2s
- LINN GEAR Uzatılmış Adım Tip A Küçük Rulo Dişlileri, 2080 Zincir
- ALLEGRO SAFETY Statik Olarak İletken EX Kanalları